TOPIC: Extreme Conditions

For over a century, the world’s most extraordinary and complex construction and industrial projects have relied on Victaulic’s innovative mechanical joint pipe systems for extreme conditions to withstand the most physically demanding environments and last the life of the build. Whether on or below ground, in the air, or underwater, Victaulic’s mechanical pipe joining solutions give engineers, site owners, and contractors the versatility and freedom of design to make the impossible possible. View More

From the world’s tallest buildings, deepest mines, and complex underwater structures, to mission-critical facilities and groundbreaking mega projects, Victaulic is the partner of choice when extreme conditions demand pipe joining systems engineered with confidence to endure even in the harshest settings. This collection of blog posts details the length that Victaulic’s engineers and products can go to successfully support our customers in some of the most difficult circumstances.

View Less
Lihir Mine uses Victaulic Vic-Press™ products for stainless steel piping

Systèmes de tuyauterie en acier inoxydable pour les chantiers miniers éloignés

Stainless steel piping has a long history on mine sites. The robust, corrosion-resistant material is ideal for mine process piping systems.

Austin Aerial Skyline- Victaulic Cooling Tower Project

Les solutions PEHD simplifient le remplacement d'une tour de refroidissement pour les installateurs locaux

Victaulic HDPE solutions helped Shoemaker Mechanical with cooling tower replacement in less time than traditional joining methods.

Victaulic HDPE Mechanical Pipe Joining System Solution mechanical joints designed & tested to withstand pipe movement caused by temperature fluctuations

How can Victaulic Products Help HDPE Pipe Beat the Heat?

In 2017 when the Glencore Oaky Creek coal mine was set to install an 8km, large-diameter HDPE raw water pipeline Glencore chose a new pipe joining ...

essais d'endurance au feu pour raccords de tuyauterie

Irons In the Fire: Fire Endurance Testing for Pipe Fittings

Mechanical pipe couplings tend to outperform other pipe joining methods in fire endurance testing for pipe fittings because they have a unique adva...

Construction Workers - Shinn Tunnel

Piping Partnership Helps Seattle Contractor Finish Tunnel Project in Ten Weeks

Partnering with Milwaukee & Victaulic, Shinn Mechanical installed, tested & completed a two-mile drain piping system in Seattle SR 99 tunnel in ten...

Préparation de tuyauteries sous-marines avec collier Victaulic

Victaulic Solves Extreme Subsea Condition

Victaulic tackles extreme subsea condition to help bring Santa Barbara Desalination Facility back online in record time.

blank road warning sign in front of storm cloud background

Comment se préparer aux changements climatiques dans le centre des données

In this post Victaulic discusses steps you can take to prepare your data center cooling system for the future predicted increase usage resulting in...

Serveur du centre de traitement des données et entrepôt de stockage en feu

How many barbeque grills fit in your data center?

Details and additional information from Victaulic on what constitutes piping solutions for high density data center cooling.