Chattez avec nous, activé par LiveChat

DÉMYSTIFICATION DE L'ASSEMBLAGE DE PEHD : MYTHE N°2 – LA FUSION CRÉE DES JOINTS PLUS RÉSISTANTS

Arms holding weights - represents strength of Victaulic HDPE pipe fittings for joining HDPE pipe

DÉMYSTIFICATION DE L'ASSEMBLAGE DE PEHD : MYTHE N°2 – LA FUSION CRÉE DES JOINTS PLUS RÉSISTANTS

Posted on September 26, 2017

While fusion has traditionally been seen as the “gold standard” in strength and reliability when it comes to joining high-density polyethylene (HDPE), empirical data suggests a change in thought is warranted.

Historically assumed to be as strong as the pipe, the integrity of fused joints is at the mercy of many variables. A fused joint is only as good as the technician operating the fusion machinery and tediously following a detailed process that leaves little room for fluctuations in environmental conditions. Surface contamination, windy, hot, or cold conditions, heating plate temperature control, and fusion times can all impact the integrity of a fused joint – and there is no visual or effective non-destructive method to inspect the quality. According to Dr. Chris O’Connor’s Polyethylene Pipeline Systems – Avoiding the Pitfalls of Fusion Welding, the existing non-destructive testing methods, such as radiography and ultrasound, “cannot reliably detect key issues that are known to affect HDPE joint quality such as fine particulate contamination, cold fusion in butt welds, or misalignment and contamination in electrofusion joints”. Once the fusion process is completed, only time will tell how well the joint is fused.  To ensure the integrity of a fuse in the absence of any effective testing, equipment must be regularly inspected and properly maintained to record accurate temperatures and calculate appropriate heating and cooling times. A culture of continued training and professional development is crucial, limiting equipment operation to only those installers that have been trained and certified, and relying heavily on user competency to ensure that the processes are strictly followed.

Unlike fusion, Victaulic’s Refuse-to-Fuse™ mechanical joints use simple tools for installation, leaving virtually no room for error. The easy four-step process can be completed regardless of weather conditions and provides visual verification of correct installation – and joint integrity. By simply visually confirming metal to metal contact at the bolt pad, the installer can verify a leak-free seal. Ultimately, high-quality joints are not only easier to achieve using the Refuse-to-Fuse system, but also easier to verify than a fused joint.

Refuse-to-Fuse mechanical joints are fully restrained joints that have been proven to meet or exceed HDPE pipe pressure ratings, allowable tensile loads and bend radius recommendations of a fused joint. This means you can push, pull and drag your pipe like any fused solution:

Refuse-to-Fuse is specifically designed with strength and durability in mind. In fact, under extreme pressure tests, Victaulic mechanical joints have been shown to outlast HDPE pipes – meaning the pipe itself will fail under pressure before a properly installed Refuse-to-Fuse joint:

To learn more about Refuse-to-Fuse system performance, click here.

Victaulic

Victaulic

Victaulic is the leading producer of mechanical pipe joining solutions. Engineered with confidence, our solutions put people to work faster, while increasing safety, ensuring reliability and maximizing efficiency.

Related posts

Victaulic StrengThin Piping System

Victaulic Adds Plug Valve to StrengThin™ Piping System, Updates Grooved Coupling Design

Victaulic StrengThin Piping System now has an updated coupling design. This innovative high-pressure piping system solution for balance-of-plant ap...

Victaulic Booth at the AHR Expo

Victaulic Heads for the 2015 AHR Expo With New Grooved Pipe Joining Products and Technologies that Lead the HVACR Industry

Visit Victaulic at the 2015 AHR Expo in Chicago. Learn about our new grooved pipe joining products & technologies including industry-leading valve ...

Victaulic Compact Hydronic Balancing Valve

Victaulic Releases Compact, Precise Hydronic Balancing Valve from IMI TA

Victaulic releases a compact precise hydronic balancing valve. The new Compact Pressure Independent Balancing & Control Valve (Compact-P) TA Series...

Recent posts

Large Pipe Retrofitting Job - Victaulic Best Practices - Tip Four

The Top Six Mechanical Retrofitting Best Practices – Tip Four

Interested in mechanical retrofitting best practices? Learn about the top six here here. Tip 4: Maximize Jobsite Productivity.

CSE 2019 Product of the Year - two Victaulic products are fiinalists

Victaulic Named Two-Time 2019 CSE Product of the Year Finalist

Starting now through Friday, June 28, CSE magazine subscribers can vote for their favorites and the 2019 winners. Click to view Victaulic’s finalists.

Mercedes Benz Stadium, Atlanta GA - Victaulic Innovative Piping Solutions

Innovative Piping Solutions Win Big at Mercedes-Benz Stadium

Victaulic innovative stadium piping solutions helped Tebarco Mechanical accommodate tight timelines and unique architecture at Mercedes-Benz Stadium.